Products made of plastic are an integral part of our everyday life. However, they often have a bad image as plastic is first and foremost associated with waste in public life. Just think of bottles of soft drinks and plastic bags that stick out of piles of rubbish or accumulate on beaches. There is no question that there should be greater awareness of the use of plastic in consumer products and that it can be restricted in many areas of life, such as when we buy fresh fruit or vegetables. But what about plastics in industry? How important are they there?
Functional components made of plastic are playing an increasingly greater role in industry. The material is very versatile in that it can be used for purposes that metal cannot be or not to the same extent. As a result of this and their optimised frictional properties, plastics from igus, used for bearings or energy chains, have an especially long service life, which is also predictable.
But every energy chain comes to the end of its service life sometime. Previously, users disposed of chains as a part of industrial waste, at best. In such a situation, it is doubtful that re-usable granulate material can be obtained, given the expense of unmixing materials for recycling. Where the end of the useful life of plastics in industry is concerned, their environmental record is therefore often not much better than that of plastics in private households.
Have your energy chain processed as part of the igus chainge Recycling Program - no matter which manufacturer they came from.
You can send us your old plastic energy chains instead of simply disposing of them with other products as part of your industrial waste. The highlight: we accept all energy chains, even from other manufacturers. We collect the returns with the goal to maximise recycling, either in our own production or by using a recycling partner, who can re-use the material. We separate the material on site and shred everything we can use for production into regranulate. We reward your commitment with an igus voucher based on the weight of the chain sent to us.
Remove the rough dirt from the energy chain, with a high-pressure cleaner, for example.
Weigh the energy chain.
Fill in the form in order to get in touch with us.
Package the energy chain and send it to us post-paid.
Address:
igus GmbH
chainge Recycling Program
Spicher Straße 1a
51147 Cologne, Germany
You will receive a voucher that you can then use for new igus products. Currently, we reward you to the value of 53 cents per kilogramme.
Example of calculation for a payment as an igus voucher: 50kg x €0.53 = €26.50 payment
"With their chainge programme, igus also fit in with Hydro's company philosophy. We lower the CO2 footprint of aluminium production with recycled consumer scrap."
Sören Hantke, Maintenance Engineer at Hydro Extrusion Germany
"Everything we do for our environment, is well-invested capital. Especially in the recycling area, we can save resources. The return process was simple and straightforward. "
Helmut Rath, Head of Control Engineering at IBG Automation about the igus recycling programme
Find out more about sustainability at igus, the ISO standard 14001 and environmental projects that we support.
Very different installation spaces and environments. Large product selection – find the right solution at once. With a 36-month guarantee.
With two to six parameters, you will receive a statement of the expected service life of the e-chain for gliding and unsupported applications.