Change Language :
"Today we can say that they are proving their worth. So far, we have not had any complaints."
Franz Eckert, design manager, on the decision to use iglidur® bearings.
JUM linear plain bearings made of the material iglidur® J show their strength in the area of seat depth adjustment, a purely linear movement. Due to the special web structure, they are predestined for linear movements, have a low coefficient of friction and, with stainless steel as a mating partner, have the very good running and noise behaviour required in the long term. "The dreaded stick-slip effect does not occur at any point," says the design manager, emphasising a key aspect. "All settings work reliably and silently."
The absence of lubrication is another positive aspect. The high-quality office chair is available in countless variants and is assembled at the company site according to customer specifications. "As the fitter no longer has to grease anything, the risk of unintentionally soiling the very high-quality seat or backrest upholstery is reduced," comments Eckert.

Corinna Graf (Nowy Styl) and Bernhard Hofstetter (igus) with the innovative design of Galileo the office chair
In the executive chair, which has been on the market since 2006, only standard plain bearings from the extensive igus® modular system, which has the right bearing for almost every application, are used. Special solutions for plain bearings should be avoided from the outset in order to concentrate on the main issue - the ergonomics of the chair. Extensive sampling and technical consultations took place in the run-up to development.
The bearing was then subjected to a variety of tests on our own test rig. The main focus here was on smooth running behaviour, low noise levels, robustness and durability. "But only real on-site use shows whether all requirements are met," says Eckert. "Today we can say that they are proving their worth. So far, we haven't had any complaints." The decision in favour of the plastic bearings has also paid off in terms of cost-effectiveness. The savings achieved by using the igus® bearings are estimated at around 50 per cent.
Here you can find the products used
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr