Change Language :

Coefficient of friction of iglidur materials with Cf53 shaft, rotating
iglidur plain bearings are self-lubricating with the addition of solid lubricants. The solid lubricants lower the coefficient of friction of the plain bearings and thus increase the wear resistance.
The coefficient of friction μ is proportional to the normal force and describes which force is needed to move a body in relation to another. Depending on whether an application is starting from a stationary position or the movement is in progress and needs to be maintained, a distinction is made between a static coefficient of friction and a dynamic coefficient of friction.

Coefficient of friction of the iglidur plain bearings at the recommended shaft surface finish and low load, p = 0.75 MPa
Shown here is the relationship between coefficient of friction and surface finish of shaft materials. It is clearly shown that the amount of friction is composed of different factors.
If the shaft is too rough, abrasion levels play an important role. Small areas of unevenness that can interlock with each other must be worn off the surface. When the surfaces are too smooth, however, higher adhesion results, i.e. the surfaces stick to each other. Higher forces are necessary to overcome the adhesion, which results from an increased coefficient of friction.
The stick-slip effect can be the result of a large difference between static and dynamic friction and of a higher adhesive tendency of mating surfaces. It also occurs due to intermittent running behaviour and can result in loud squeaking. People have observed over and over again that these noises do not occur or can be eliminated with rough shafts. With applications with great potential for the stick-slip effect, such as those involving slow movements or large resonance of the housings, it is important to pay attention to the optimal surface finish of the shafts.
Have you not found the iglidur material you are looking for? You can find extensive data on all materials and data sheets in our online shop.
In person:
Monday to Friday from 7 am - 8 pm.
Saturdays from 8 am- 12 pm.
Online:
24h
WhatsApp-Service:
Montag – Freitag: 8 – 16 Uhr